This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问C3100中例子Http server中POST方式如何取得返回值?



我在底层返回GET没问题,但返回POST是web页面显示无内容。

下位机代码

if(pal_Memcmp(ptr, CAN_POST_token, pal_Strlen(CAN_POST_token)) == 0){

  processCANsend(ptr);

  ptr = pResponse->ResponseData.token_value.data;

  pResponse->ResponseData.token_value.len = 0;

 pal_Strcpy(ptr, "{\"id\"=182,\"data\"=\"30 31 32 33 34 35 36 37\"}");

pResponse->ResponseData.token_value.len += pal_Strlen(ptr);

}

上位机代码:

function SendPacket1()

{

var params = "__SL_P_UCA="//"__SL_P_UDW=";

params += document.getElementById("CAN_ID").value;

params += ",";

params += document.getElementById("CAN_Data").value;

params += ",";

HTTPrequest.open("POST","No_content", true);

HTTPrequest.setRequestHeader("Content-type", "application/x-www-form-urlencoded");

HTTPrequest.setRequestHeader("Content-length", params.length);

HTTPrequest.setRequestHeader("Connection", "close");

HTTPrequest.onreadystatechange = function()

{

if (HTTPrequest.readyState==4 && HTTPrequest.status==200)

{

            text1 = HTTPrequest.responseText;

}

}

HTTPrequest.send(params);

}

监控所得,下位机确实运行代码了,但web返回状态为204


  • HTTP的状态码有很多种,主要有1xx(临时响应)、2xx(成功)、3xx(已重定向)、4xx(请求错误)以及5xx(服务器错误)五个大类,每个大类还对应一些具体的分类。平时我们接触比较多的是200、400、500等。

    这里我们主要讨论一下状态码204,在HTTP RFC 2616中关于204的描述如下:

    If the client is a user agent, it SHOULD NOT change its document view from that which caused the request to be sent. This response is primarily intended to allow input for actions to take place without causing a change to the user agent’s active document view, although any new or updated metainformation SHOULD be applied to the document currently in the user agent’s active view.
    意思等同于请求执行成功,但是没有数据,浏览器不用刷新页面.也不用导向新的页面。如何理解这段话呢。还是通过例子来说明吧,假设页面上有个form,提交的url为http-204.htm,提交form,正常情况下,页面会跳转到http-204.htm,但是如果http-204.htm的相应的状态码是204,此时页面就不会发生转跳,还是停留在当前页面。另外对于a标签,如果链接的页面响应码为204,页面也不会发生跳转。

    所以对于一些提交到服务器处理的数据,只需要返回是否成功的情况下,可以考虑使用状态码204来作为返回信息,从而省掉多余的数据传输。

    POST用于给服务器发送隐性数据使用的,不会出现在http上,服务器那边可以接收到