CC3200在用Pinmux配置引脚时,想将暂时不用的GPIO口配置为Low Power Deep Sleep模式,请问GPIO引脚的配置该如何设置?或者请问有没有参考例程呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CC3200在用Pinmux配置引脚时,想将暂时不用的GPIO口配置为Low Power Deep Sleep模式,请问GPIO引脚的配置该如何设置?或者请问有没有参考例程呢?
低功耗深度睡眠(LPDS)模式是 CC3200 中 Cortex-M4 核的一种重要的低功耗睡眠模式。
关于LPDS模式,建议您先看一下
http://www.ti.com.cn/cn/lit/an/zhca635/zhca635.pdf
以及
https://e2e.ti.com/support/embedded/tirtos/f/355/p/574775/2119936#pi317008filter=all&pi317008scroll=false
参考如下代码
//****************************************************************************
//
//! Enter the HIBernate mode configuring the wakeup timer
//!
//! \param none
//!
//! This function
//! 1. Sets up the wakeup RTC timer
//! 2. Enables the RTC
//! 3. Enters into HIBernate
//!
//! \return None.
//
//****************************************************************************
void EnterHIBernate()
{
#define SLOW_CLK_FREQ (32*1024)
//
// Configure the HIB module RTC wake time
//
MAP_PRCMHibernateIntervalSet(5 * SLOW_CLK_FREQ);
//
// Enable the HIB RTC
//
// MAP_PRCMHibernateWakeupSourceEnable(PRCM_HIB_SLOW_CLK_CTR);
//------------------------------------------------------------Hib模式下增加GPIO唤醒---------------------------------------------------------------
// PRCMHibernateWakeupSourceEnable入口参数
// PRCM_HIB_SLOW_CLK_CTR -PRCM_HIB_GPIO2 -PRCM_HIB_GPIO4 -PRCM_HIB_GPIO13 -PRCM_HIB_GPIO17 -PRCM_HIB_GPIO11 -PRCM_HIB_GPIO24 -PRCM_HIB_GPIO26
PRCMHibernateWakeupSourceEnable(PRCM_HIB_GPIO13);
PRCMHibernateWakeUpGPIOSelect(PRCM_HIB_GPIO13,PRCM_HIB_FALL_EDGE); //按键按下去产生上升沿,松开后产生下降沿!注意入口参数的顺序!!!
//------------------------------------------------------------------------------------------------------------------------------------------------
// DBG_PRINT("HIB: Entering HIBernate...\n\r");
UART_PRINT("Entering HIB\n\r");
MAP_UtilsDelay(80000);
//
// powering down SPI Flash to save power
//
Utils_SpiFlashDeepPowerDown();
//
// Enter HIBernate mode
//
MAP_PRCMHibernateEnter();
}
// set_rtc_as_wk_src(WK_LPDS, LPDS_DUR_SEC, false); //测试LPDS功耗,不使用定时器唤醒,仅使用GPIO唤醒!
// set_gpio_as_wk_src(WK_LPDS, GPIO_SRC_WKUP, PRCM_LPDS_FALL_EDGE);
//------------------------------------------------------------------注意!!---------------------------------------------------------------------------------------------
// set_gpio_as_wk_src(WK_HIB, GPIO_SRC_WKUP, PRCM_LPDS_FALL_EDGE); //必须设置进入Hib模式下的中断唤醒源,否则无法进入Hib模式
//注意在sl_Stop(10)之前不要启动该语句,否则NWP在sl_Stop(10)之后就自动进入了Hib模式但是唤醒源并没设置OK,直接屏蔽该语句,用EnterHIBernate();即可
// 对应低功耗模式:
// e_pm_S0, // CPU & HW modules are functioning at optimal & intended freq Active模式
// e_pm_S1, // CPU is halted, high freq PLL CLK is available to HW modules Sleep模式
// e_pm_S2, // CPUSS is clk gated, Mid freq CLK is availalbe to HW modules DPS模式
// e_pm_S3, // SoC almost pwr off, slow CLK is present & OCRAM is retained LPDS模式
// e_pm_S4 // SOC almost pwr off, slow CLK is present & few regs retained hib模式