This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200/CC3220 Provisioning Smartconfig

Other Parts Discussed in Thread: CC3200

您好,

关于CC32XX系列说在smartconfig时不支持5Ghz和mimo的AP device。因为现在手机或者AP都是支持MIMO模式的,要怎么解决这个匹配不成功的问题呢

另外如果有大神能解释下CC3220比CC3200在smartconfig时性能提高在哪里就更好了

  • If your phone is connected to Wi-Fi in 5 GHz band or in MIMO mode, SmartConfig will not work. It is also known to some devices that Smart Config does not work even though the network is running 2.4GHz SISO. TI recommends always using a backup provisioning solution in case the first method fails. Please visitfor more details.