This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC3220SF例程中network terminal的一些疑问

Other Parts Discussed in Thread: CC3220SF, CC3200

1.问题一:

最近在测试network terminal例程,我用路由器将PC和CC3220SFdemo板组局域网,我的PC的IP地址:192.168.1.100,CC3220SFdemo的IP 地址:192.168.1.101. 根据贵公司例程提示,我使用send命令,串口端返回数据包发送成功,使用ping指令也能验证PC和CC3220SFdemo都在局域网内。

我的问题是:如果我现在要使用CC3220SFdemo (client)板走TCP/IP协议,发送“hello”到PC端(server, IP:192.168.1.100,Port=8080)的网络调试助手端,应该使用哪个例程或指令?

我如何对CC3220SFdemo 的某个Port(如IP:192.168.1.100,Port=8080)进行监听,接收由PC(server, IP:192.168.1.100,Port=8080)发送来的数据?

2.问题二:

CC3220SFdemo是否可以同时处于AP和STA模式?