调试3200-LAUNCHXLA,下载例程UDP,一直可以正常连接发包,直至最近调试一直是下面串口显示,AP和BSSID均显示为空,这个之前是有信息的,AP显示可以连接,但数据不正常丢包严重。
出现该现象之前做过格式化片外FLASH操作,但在线调试应该和片外FLASH无关。
以下是串口输出,希望能够得到答案,谢过。
Host Driver Version: 1.0.1.6
Build Version 0.0.0.0.31.0.0.0.0.0.0.0.0
Device is configured in default state
Device started as STATION
Connecting to AP: cc3200demo ...
[WLAN EVENT] STA Connected to the AP: , BSSID: 0:0:0:0:0:0
[NETAPP EVENT] IP Acquired: IP=192.168.43.104 , Gateway=192.168.43.1
Connected to AP: cc3200demo
Device IP: 192.168.43.104