This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200电源问题

Other Parts Discussed in Thread: CC3200

求救CC3200电源问题,问题如下:

CC3200是3.3V供电的,板子贴好后,CC3200的几路电源如下(用万用表量的):VDD_ANA = 1.91V; VDD_DIG_CC = 1.25V;VDD_PA 很奇怪,一直变化的,最低0.01V,高的时候0.45V,通常在0.04V,由于没有示波器,所以不知道VDD_PA的变化。请问以上电压是否正确?

原理图如下:cc3200-v1-原理图.pdf