This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220S Gang image

Other Parts Discussed in Thread: CC3200

请问 datasheet中的Gang image时什么意思?

应该如何理解?



  • 具体请参考:
    processors.wiki.ti.com/.../CC3200_Production_Line_Guide



    Gang image – Use a special binary image that is written directly to the serial flash, that the CC3200 can use to create the desired contents of the serial flash.

  • 这里的Gang有可能是从msp Gang 编程器的概念里出来的
    The gang image may be programmed to the serial flash device after assembly on the board provided some considerations are taken:

    The serial flash SPI interface pins must be brought out for physical contact with the programmer (e.g. male headers, test pads)
    The SPI lines must not be driven by any other source while programming.
    The CC3200 will be held in reset during programming to prevent contention.
    一般单片机的烧录文件都可以叫image。