This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

idle_profile demo中, 如何添加对UART1的使用



在idle_profile demo中,添加UART1模块,添加方式如下:

在main方法中,添加gpio的初始化:

    MAP_PRCMPeripheralClkEnable(PRCM_UARTA1, PRCM_RUN_MODE_CLK);
    //
    // Configure PIN_16 for UART1 UART1_TX
    //
    MAP_PinTypeUART(PIN_01, PIN_MODE_7);
    //
    // Configure PIN_17 for UART1 UART1_RX
    //
    MAP_PinTypeUART(PIN_02, PIN_MODE_7);
然后添加cc_hndl g_tUartHndl1,
tUartHndl1 = uart_open(PRCM_UARTA1)
====================================================================
然后执行uart_read(g_tUartHndl1, buf, buf_size); uart_write(g_tUartHndl1, buf, buf_size) (执行前 已经从LPDS模式唤醒)
测试后,发现无法向uart1 发送和读取数据。
请大家帮忙看看,是否使用有误,或者需要如何操作? 谢谢!