This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc3220 使用spi+dma 采外挂adc数据



看reference manual 4.1上写的是

•Data sizes of 8, 16, and 32 bits

• Transfer size is programmable in binary steps from 1 to 1024 

意思是可以每次传8/16/32位的数据,FIFO可以存1024个数据(不论多少位)吗?

8.5.3关于spi的FIFO Mode要怎么理解?

现在的需要是通过gspi+dma来取数据,外挂adc每次需要给18个时钟,可以配置成这样吗?还是说必须给32bit再从中取?一次要连采1024个数据,dmaFIFO的地址如何定义?另外gspi 速度可以到多少?