Other Parts Discussed in Thread: CC3200, CC3220SF, CC1310
我手头只有CC3200的 Launchpad 板子
把CC3200换上CC3220SF后,
用CC1310 Launchpad 上的 XDS110调试CC3220SF?
我的 XDS110连不上CC3220SF?出错!
那能不能用CC1310 Launchpad 上的 XDS110调试CC3220SF?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以,
The jumper block in the middle of the board can be used to disconnect the upper section (XDS110 debugger) from the bottom section (CC1310). The jumpers are mounted by default. If you want to debug the CC1310 from an external debugger, you need to remove all the jumpers and connect the debugger to the socket marked CC1310 In.
It is also possible to use the LaunchPad to debug external targets. In this case, remove all the jumpers and connect the external target to the socket marked XDS110 Out.
The jumper block marked VSENSE can be used to select the source of power to the CC1310. Usually, power is supplied from USB and a jumper is mounted in the position marked XDS110 power (factory default). If you want to power CC1310 from an external supply, move the jumper to the position marked Extern. Pwr, and connect the external supply to the 3V3 pin on J1. Also make sure to remove the 3V3 jumper from the main jumper block. Make sure that the voltage applied stays within the supply range of the CC1310.
用CC1310上面的 XDS110来调试CC3220SF,为上面JTAG 口上的 RST脚没有信号控制输出给CC3220SF?
一直处于上拉
直接用CC1310板子调试板上CC1310,该RST脚有下来脉冲信号