Other Parts Discussed in Thread: UNIFLASH, CC3200, CC3100, CC3100SDK, CC3100BOOST
sdk和服务包都是最新版的,刚开始能用,后来使用uniflash时点击了operation里的generate config binares以后,就不能用了,我后来又尝试刷新固件库还是不想,运行例子总是出现一个标题以后就是general even 就没反应了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: UNIFLASH, CC3200, CC3100, CC3100SDK, CC3100BOOST
sdk和服务包都是最新版的,刚开始能用,后来使用uniflash时点击了operation里的generate config binares以后,就不能用了,我后来又尝试刷新固件库还是不想,运行例子总是出现一个标题以后就是general even 就没反应了。
我用的 编译环境是Code Composer Studio 9.0.0 CC3100_CC3200_ServicePack_1.0.1.14-2.12.2.8 CC3100SDK_1.3.0 CC3100SDK_1.3.0 原因我找到了,是因为更新serviceopack的时候没有操作好,在更行servicepack的时候,需要按sw2进行重置,论坛上好多遇到sl_Start卡死应该也是这个问题,不过我还是有个疑惑,我不知道怎样更行固件库才算成功,servicepack每烧写成功以后里面出现的是
[08:31:29] INFO: file start size fail total size filename
[08:31:29] INFO: index block [BLKs] safe [BLKs]
[08:31:29] INFO: ----------------------------------------------------------------------------
[08:31:29] INFO: N/A 0 5 N/A 5 FATFS
[08:31:29] INFO: 4 5 66 no 66 /sys/servicepack.ucf
[08:31:29] INFO:
[08:31:29] INFO: Flash usage
[08:31:29] INFO: -------------------------
[08:31:29] INFO: used space: 71 blocks
[08:31:29] INFO: free space: 185 blocks
[08:31:29] INFO: memory hole: [71-255]
[08:31:29] INFO: > Executing Operation: Disconnect
[08:31:29] Operation ListFileSystem returned.
如果出现这个,就会出现上述情况,但是uniflash没有报错什么的,但是有时操作的时候更新servicepack
后会出现错误
08:35:29] INFO:
Verification OK
[08:35:30] INFO: Downloading file "/sys/servicepack.ucf" with size 38160
[08:35:30] ERROR: Open operation failed
[08:35:30] INFO: > Executing Operation: Disconnect
[08:35:30] Operation ServicePackProgramming returned.
然后查了一下
[08:35:40] INFO: file start size fail total size filename
[08:35:40] INFO: index block [BLKs] safe [BLKs]
[08:35:40] INFO: ----------------------------------------------------------------------------
[08:35:40] INFO: N/A 0 5 N/A 5 FATFS
[08:35:40] INFO: 4 5 1 yes 2 /sys/stacfg.ini
[08:35:40] INFO: 6 7 1 yes 2 /tmp/fcon.frm
[08:35:40] INFO: 7 9 1 yes 2 /tmp/fcon.ssid
[08:35:40] INFO: 8 11 1 yes 2 /sys/pref.net
里面是这个样子的,此时那些例子就能正常运行。虽然能正常运行,但是当我遇到httpservice时,更新到里面的网页打不开,不知道为什么,
[08:47:47] INFO: 4 5 1 no 1 www/index.html
[08:47:47] INFO: 6 6 1 no 1 www/blink_led.html
这里面的yes和no'代表的是烧录是否成功,
谢谢
[10:48:36] Begin ServicePackProgramming operation.
[10:48:37] INFO: > Executing Operation: Connect
[10:48:39] INFO: setting break signal
[10:48:40] INFO: detecting FTDI for device reset
[10:48:41] INFO: connection succeeded
[10:48:41] INFO: getting storage list
[10:48:41] INFO: > Executing Operation: ServicePackProgramming
[10:48:41] INFO: Path to the service pack file: C:/TI/CC3100_CC3200_ServicePack_1.0.1.14-2.12.2.8/servicepack_1.0.1.14-2.12.2.8.bin
[10:48:41] INFO: reading version info
[10:48:41] INFO: CC3100Z Device detected.
[10:48:41] INFO: NWP/MAC/PHY Version from Service Pack:
[10:48:41] INFO: NWP version: 0.0.0.0
[10:48:41] INFO: MAC version: 0.0.0.0
[10:48:41] INFO: PHY version: 0.0.0.0
[10:48:41] INFO: reading version info
[10:48:41] INFO: DEVICE CC3100 ES1.32
[10:48:41] INFO: reading version info
[10:48:43] INFO: downloading NWP CODE
[10:48:43] INFO: Erase storage FLASH
[10:48:43] INFO: erase storage succeeded
[10:48:43] INFO: erase storage completed
[10:48:44] INFO: Verifying Data...
[10:48:44] INFO:
Verification OK
[10:48:45] INFO: Downloading file "/sys/servicepack.ucf" with size 38160
[10:48:50] INFO:
New Token is 0x0
[10:48:50] INFO: Download complete
[10:48:50] INFO: > Executing Operation: Disconnect
[10:48:51] Operation ServicePackProgramming returned.
nwp,mac和phy地址都是0,这是为什么。并且运行什么例子都是不能运行的,只能出现一个标题,这是因为我的servicepack坏了吗,我用的也是最新版的和你的一样,对了,我的设备是CC3100+f5529,能不能让我看看你点击list file system出现的内容。