Other Parts Discussed in Thread: CC3220SF
开发板:CC3220SF Lanuchxl 例程:MQTT_client_server
SDK:simplelink_cc32xx_sdk_4_20_00_07
hi!你们好,我在使用 CC3220SF 导入例程 rtos/CC3220SF_LAUNCHXL/demos/MQTT_client_server 后,设置好 AP 连接的参数(本地wifi账号密码) , 烧写进开发板后终端上总显示代理连接失败,连本地的客户端好像也连接失败了,我该如何作出调整才能连接成功呢?
终端显示:
============================================
MQTT client server Example Ver: 1.1.1
============================================
CHIP: 0x30000019
MAC: 2.0.0.0
PHY: 2.2.0.7
NWP: 3.16.0.1
ROM: 0
HOST: 3.0.1.65
MAC address: 98:84:e3:f6:61:9a
============================================
*************************************************
CC32xx MQTT client server Application
*************************************************
Device came up in Station mode
[WLAN EVENT] STA Connected to the AP: hopetruly , BSSID: 78:11:dc:46:c5:d
[NETAPP EVENT] IP acquired by the device
Device has connected to hopetruly
Device IP Address is 192.168.31.51
...........Connection to broker failed, Error code: -111
BRIDGE DISCONNECTION
On-board Client Disconnected
In order to reconnect local client, Reset board.
.
如果有人能帮助我,我将感激不尽!