Other Parts Discussed in Thread: CC3220SF
SDK:simplelink_cc32xx_sdk_4_20_00_07 开发板:官方CC3220SF
起步例程:uartecho
在我实验完uartecho后,我尝试着自己写一个uart驱动,使用的回调模式,但奇怪的是,无论我发多少次数据,读回调中断始终没有触发,逻辑分析仪上可以看到TX发送的数据,为此我有些问题想请教:
1. 发送数据是否有数据格式?垃圾数据难道不能发送成功吗?如果有标准格式,那会是什么样的呢?
2. 我查看相关文档的时候,我注意到当FIFO被填满的时候中断也会触发,但实际情况是无论我发送多少次数据我都没办法触发读回调
3. 我的初始化配置是否正确?我的目的是想让两块CC3220SF互相通过uart通信。(使用了UARTDMA)
4. 感激不尽,望能一一解答,下面附上我的代码
static const UARTCC32XXDMA_HWAttrsV1 uartCC32XXHWAttrs0 = {
.baseAddr = UART0_BASE,
.intNum = INT_UART0,
.intPriority = (~0),
.flowControl = UARTCC32XXDMA_FLOWCTRL_NONE,
.rxChannelIndex = UDMA_CH8_UARTA0_RX,
.txChannelIndex = UDMA_CH9_UARTA0_TX,
.rxPin = UARTCC32XXDMA_PIN_45_UART0_RX,
.txPin = UARTCC32XXDMA_PIN_62_UART0_TX,
.ctsPin = UARTCC32XXDMA_PIN_UNASSIGNED,
.rtsPin = UARTCC32XXDMA_PIN_UNASSIGNED,
.errorFxn = NULL
};
/*
* ======== uartecho.c ========
*/
#include <stdint.h>
#include <stddef.h>
/* Driver Header files */
#include <ti/drivers/GPIO.h>
#include <ti/drivers/UART.h>
#include <ti/posix/ccs/unistd.h>
/* Driver configuration */
#include "ti_drivers_config.h"
#define MAX_NUM_RX_BYTES 30 // Maximum RX bytes to receive in one go
#define MAX_NUM_TX_BYTES 30 // Maximum TX bytes to send in one go
uint32_t wantedRxBytes; // Number of bytes received so far
uint8_t rxBuf[MAX_NUM_RX_BYTES]; // Receive buffer
uint8_t txBuf[MAX_NUM_TX_BYTES]; // Transmit buffer
UART_Handle uart;
int32_t readCount;
uint8_t sendbuffer[20] = {0x40,0x10,0x40,0x10,0x40,0x10,0x80,0x20,0x80,0x20,0x80,0x20,0x80,0x20,0x80,0x20,0x20,0x20};
uint8_t recvicebuffer[16];
int c;
size_t i ;
void gpioButtonFxn0(uint_least8_t index)
{
UART_write(uart, &sendbuffer, wantedRxBytes);
}
// Write callback function
static void writeCallback(UART_Handle handle, void *rxBuf, size_t size)
{
// Do nothing
}
// Read callback function
static void readCallback(UART_Handle handle, void *rxBuf, size_t size)
{
GPIO_toggle(CONFIG_GPIO_LED_0);
// Make sure we received all expected bytes
if (size == wantedRxBytes) {
// Copy bytes from RX buffer to TX buffer
for ( i = 0; i < size; i++)
txBuf[i] = ((uint8_t*)rxBuf)[i];
// Echo the bytes received back to transmitter
UART_write(handle, txBuf, size);
// Start another read, with size the same as it was during first call to
// UART_read()
UART_read(handle, rxBuf, wantedRxBytes);
GPIO_toggle(CONFIG_GPIO_LED_1);
}
else {
// Handle error or call to UART_readCancel()
}
}
/*
* ======== mainThread ========
*/
void *mainThread(void *arg0)
{
//char input;
const char echoPrompt[] = "Echoing characters:\r\n";
UART_Params uartParams;
/* Call driver init functions */
GPIO_init();
UART_init();
/* Configure the LED pin */
GPIO_setConfig(CONFIG_GPIO_LED_0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);
GPIO_setConfig(CONFIG_GPIO_LED_1, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);
GPIO_setConfig(CONFIG_BUTTON_0, GPIO_CFG_IN_PU | GPIO_CFG_IN_INT_FALLING);
/* Turn on user LED */
GPIO_write(CONFIG_GPIO_LED_0, CONFIG_GPIO_LED_OFF);
GPIO_write(CONFIG_GPIO_LED_1, CONFIG_GPIO_LED_OFF);
/* Install Button callback */
GPIO_setCallback(CONFIG_BUTTON_0, gpioButtonFxn0);
/* Enable interrupts */
GPIO_enableInt(CONFIG_BUTTON_0);
/* Create a UART with data processing off. */
UART_Params_init(&uartParams);
uartParams.writeMode = UART_MODE_CALLBACK;
uartParams.writeDataMode = UART_DATA_BINARY;
uartParams.writeCallback = writeCallback;
uartParams.readMode = UART_MODE_CALLBACK;
uartParams.readDataMode = UART_DATA_BINARY;
uartParams.readCallback = readCallback;
uartParams.baudRate = 115200;
uart = UART_open(CONFIG_UART_0, &uartParams);
if (uart == NULL) {
/* UART_open() failed */
while (1);
}
UART_write(uart, echoPrompt, sizeof(echoPrompt));
wantedRxBytes = 16;
int rxBytes = UART_read(uart, rxBuf, wantedRxBytes);
// UART_write(uart, echoPrompt, sizeof(echoPrompt));
/* Loop forever echoing */
while (1) {
}
}