This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3235S的功耗问题

Other Parts Discussed in Thread: CC3235S

先用sl_WlanProfileAdd添加wifi的ssid和password,再用SL_WLAN_CONNECTION_POLICY(1, 0, 0, 0)设置成自动连接,当局域网断开的时候,测得功耗为14mA,想问问这个功耗是否正常,如何能够降低局域网断开时CC3235S的功耗。

  • 手册给出的功耗:
    – 高级低功耗模式:
    – 关断:1µA,休眠:4.5µA
    – 低功耗深度睡眠 (LPDS):120μA
    – 空闲连接(MCU 处于 LPDS 状态):710μA
    – RX 流量(MCU 处于活动模式):59mA
    – TX 流量(MCU 处于活动模式):223mA

    “当局域网断开的时候,测得功耗为14mA” 是指idle模式下的功耗吗?如何测量的?