Other Parts Discussed in Thread: CC3220SF
见题。
在CC3220SF的network_terminal例程中,mainthread里面用到了wifi_Config()函数,注释说用户要根据自己的需要进行配置,那么要在哪里重新对wifi_Config()进行编码呢?
按住Ctrl+左键点击这个函数,链接到了device.h,个人觉得应该不是在device.h里面直接改动吧?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC3220SF
见题。
在CC3220SF的network_terminal例程中,mainthread里面用到了wifi_Config()函数,注释说用户要根据自己的需要进行配置,那么要在哪里重新对wifi_Config()进行编码呢?
按住Ctrl+左键点击这个函数,链接到了device.h,个人觉得应该不是在device.h里面直接改动吧?
这个是恢复为默认状态,看下下面的说明
/*! \brief Configure SimpleLink to default state. The sl_WifiConfig function allows to configure the device to a pre-configured state by sysconfig UI\ ti_drivers_net_wifi_Config.c. The configuration of the SimpleLink Wifi is usually persistent, and can be reconfigured at runtime. Reconfiguration should be performed only when needed since the process involves flash writes and might impact system lifetime (flash write endurance) and power consumption. It's important to note that this is one example for a 'restore to default state' function, which meet the needs of this application. User who wish to incorporate this function into he's app, must adjust the implementation and make sure it meets he's needs. \return Upon successful completion, the function shall return 0. In case of failure, this function would return -1. */ _i32 sl_WifiConfig();