Other Parts Discussed in Thread: CC3220R, CC3220S, CC3220SF
在可以联网的情况下,CC3220R最低能达到多少功耗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
– 高级低功耗模式: – 关断:1µA – 休眠:4.5µA
– 低功耗深度睡眠 (LPDS):135µA(测试对象 为具有 256KB RAM 保持的 CC3220R、 CC3220S 和 CC3220SF)
– RX 流量(MCU 处于活动模式):54 OFDM 时为 59mA(测试对象为 CC3220R 和 CC3220S;CC3220SF 会额外消耗 10mA)
– TX 流量(MCU 处于活动模式):在 54 OFDM、最大功耗时为 223mA(测量对象为 CC3220R 和 CC3220S;CC3220SF 会额外 消耗 15 mA)
– 空闲连接(MCU 处于 LPDS 模式):DTIM = 1 时为 710µA(测量对象为具有 256KB RAM 保持的 CC3220R 和 CC3220S