Other Parts Discussed in Thread: LAUNCHXL-CC3235SF, CC3235SF, CC2640R2F
硬件使用的是官方的LAUNCHXL-CC3235SF开发板,在运行C:\ti\simplelink_cc32xx_sdk_4_20_00_07\examples\rtos\CC3235SF_LAUNCHXL\drivers\spimaster\freertos
这个例子是发现发送可以正常发送,但是接收到的数据却不对。
于是为了排除问题我把MOSI与MISO短接到了一起,按道理应该就是发送什么接收什么了吧,但是接收还是错误的。
下面是我的代码:
/* Open SPI as master (default) */
SPI_Params_init(&spiParams);
spiParams.frameFormat = SPI_POL0_PHA0;
spiParams.dataSize = 8;
spiParams.bitRate = 1000000;
masterSpi = SPI_open(CONFIG_SPI_MASTER, &spiParams);
if (masterSpi == NULL) {
Display_printf(display, 0, 0, "Error initializing master SPI\n");
while (1);
}
else {
Display_printf(display, 0, 0, "Master SPI initialized\n");
}
/*
* Master has opened CONFIG_SPI_MASTER; set CONFIG_SPI_MASTER_READY high to
* inform the slave.
*/
GPIO_write( CONFIG_SPI_MASTER_READY, 1 );
/* Copy message to transmit buffer */
strncpy((char *) masterTxBuffer, MASTER_MSG, SPI_MSG_LENGTH);
for (i = 0; i < 1; i++) {
/*
* Wait until slave is ready for transfer; slave will pull
* CONFIG_SPI_SLAVE_READY low.
*/
GPIO_write(CONFIG_SPI_MASTER_READY, 0);
/* Initialize master SPI transaction structure */
masterTxBuffer[0] = 0x01;
masterTxBuffer[1] =0x02;
masterTxBuffer[2] =0x03;
masterTxBuffer[3] =0x04;
masterTxBuffer[4] =0x05;
memset((void *) masterRxBuffer, 0, SPI_MSG_LENGTH);
transaction.count = SPI_MSG_LENGTH;
transaction.txBuf = (void *) masterTxBuffer;
transaction.rxBuf = (void *) masterRxBuffer;
/* Toggle user LED, indicating a SPI transfer is in progress */
// GPIO_toggle(CONFIG_GPIO_LED_1);
/* Perform SPI transfer */
transferOK = SPI_transfer(masterSpi, &transaction);
if (transferOK) {
GPIO_write(CONFIG_SPI_MASTER_READY, 1);
Display_printf(display, 0, 0, "Master received:[%02x] %02x %02x %02x %02x %02x",
i,
masterRxBuffer[0],
masterRxBuffer[1],
masterRxBuffer[2],
masterRxBuffer[3],
masterRxBuffer[4]);
}
else {
Display_printf(display, 0, 0, "Unsuccessful master SPI transfer");
}
/* Sleep for a bit before starting the next SPI transfer */
}
我发送的是 5 个字节 0x01 0x02 0x3 0x04 0x05,理论上也应该收到 0x01 0x02 0x3 0x04 0x05 但是在transaction.rxBuf里收到的确是 0x03 0x0c 0x0f 0x30 0x1b。
我用逻辑分析仪也看了,在逻辑分析仪上看的数据没问题:
请教下问题可能出在哪?卡在这已经一个星期了。。。多谢!