This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个函数前面有详细说明:
/*! \brief SimpleLinkNetAppEventHandler This handler gets called whenever a Netapp event is reported by the host driver / NWP. Here user can implement he's own logic for any of these events. This handler is used by 'network_terminal' application to show case the following scenarios: 1. Handling IPv4 / IPv6 IP address acquisition. 2. Handling IPv4 / IPv6 IP address Dropping. \param pNetAppEvent - pointer to Netapp event data. \return void \note For more information, please refer to: user.h in the porting folder of the host driver and the CC31xx/CC32xx NWP programmer's guide (SWRU455) section 5.7
你可以参考'network_terminal'看看具体实现