This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF使用CCS里面的syscfg的问题

Other Parts Discussed in Thread: CC3220SF

您好,我之前使用CC3220SFlaunch开发板进行开发。现在想使用开发板给CC3220MODSF模块进行烧录,我将开发板上的烧录线RX TX,TDO TDI RST TCK TMI 直联模块,然后成功烧录。但是我发现一个问题,就是在GPIO口配置上与syscfg不一致。是这样的,我想使用MOD模块上的GPIO8口,对应MOD板子上的PIN53,但是发现烧录过去后变成了GPIO30口,一查表发现其配置还是遵循CC3220SFLaunch开发板的布局(在这里pin53对应GPIO30,我如果要使用GPIO8得改成PIN63),所以我想请问下,在CCS的软件里的syscfg是不是只适配开发板的pin口?还有,是否有其它烧录器可以烧录MOD模块?每次都需要飞线过去烧录很不方便有没批量烧录的方案