This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1805 使用?

1. 目前网关上使用型号为WL1805,网关主控为STM32mp1,实际使用2.4GHz,在近距离测试,wl1805作为STA,AP或路由器和网关都在同一位置,网关去ping AP 延时约10-20ms左右;是否正常?
2.  WL1805在2.4Ghz下MIMO双天线模式怎么使用,驱动是默认匹配还是需要配置?MIMO双天线模式是否对延时和吞吐量都有提升?目前实际测试中通过是否接天线看信号强度,判断出AN2是接天线没起作用,如果只接AN2天线,无线信号强度非常弱,和没接天线效果相近
3. 把AP调整距离网关5米左右的距离时,通过“iw dev wlan0 link”,能看到TX bitrate不是特别稳定,会有波动,如10-54.MBit/s跳动
4. 请问还有其它指令或方法可以测试吗?同时可以在自己wl1805上调整到调试模式,直接使用“WLAN 实施调优工具 (RTTT)”么?
谢谢!