Part Number: CC3220SF
Other Parts Discussed in Thread: UNIFLASH
您好,我想请问下。对于CC3220SF可否使用sl_Fs文件系统操作与其相连的片外Flash里面的文件?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
文件系统就是对SFLASH进行操作的
The SimpleLink Wi-Fi device maintains a nonvolatile file system in which the data is stored on an external
serial flash (through SPI). The file system provides the ability to organize data and access resources using
a simple host interface.
Online User Files仅在开发者模式才能使用
A device programmed with a development image allows for browsing its files, user files, and system files,
and can perform several operations listed in the following subsections.
Most system files can not be viewed in the file list, and have no read/write access.
The online browser edits the file on the device serial flash; the changes do not affect the programming
image file, which is prepared with the offline browser.