Part Number: CC3220SF
您好, 我使用CC3220SF搭配simplelink_cc32xx_sdk_4_30_00_06 进行开发,发现当启动sl_Start开启SimpleLink服务时,会默认开始所有SimpleLink服务。如何选择性的开启某些功能呢?比如我只想使用sl_File(文件系统),而不想使用WIFI。更不想开启WIFI模块。请问我应该怎么做?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC3220SF
您好, 我使用CC3220SF搭配simplelink_cc32xx_sdk_4_30_00_06 进行开发,发现当启动sl_Start开启SimpleLink服务时,会默认开始所有SimpleLink服务。如何选择性的开启某些功能呢?比如我只想使用sl_File(文件系统),而不想使用WIFI。更不想开启WIFI模块。请问我应该怎么做?
/*!
\brief Start the SimpleLink device
This function initialize the communication interface, set the enable pin
of the device, and call to the init complete callback.
\param[in] pIfHdl Opened Interface Object. In case the interface
must be opened outside the SimpleLink Driver, the
user might give the handler to be used in \n
any access of the communication interface with the
device (UART/SPI). \n
The SimpleLink driver will open an interface port
only if this parameter is null! \n
\param[in] pDevName The name of the device to open. Could be used when
the pIfHdl is null, to transfer information to the
open interface function \n
This pointer could be used to pass additional information to
sl_IfOpen in case it is required (e.g. UART com port name)
\param[in] pInitCallBack Pointer to function that would be called
on completion of the initialization process.\n
If this parameter is NULL the function is
blocked until the device initialization
is completed, otherwise the function returns
immediately.
\return Returns the current active role (STA/AP/P2P/TAG) or an error code:
- ROLE_STA, ROLE_AP, ROLE_P2P, ROLE_TAG in case of success and when pInitCallBack is NULL (the third parameter),\n
or, in case of pInitCallBack is not null - sl_start will return zero in case of success,
otherwise in failure one of the following is return:
- SL_ERROR_ROLE_STA_ERR (Failure to load MAC/PHY in STA role)
- SL_ERROR_ROLE_AP_ERR (Failure to load MAC/PHY in AP role)
- SL_ERROR_ROLE_P2P_ERR (Failure to load MAC/PHY in P2P role)
- SL_ERROR_CALIB_FAIL (Failure of calibration)
- SL_ERROR_FS_CORRUPTED_ERR (FS is corrupted, Return to Factory Image or Program new image should be invoked (see sl_FsCtl, sl_FsProgram))
- SL_ERROR_FS_ALERT_ERR (Device is locked, Return to Factory Image or Program new image should be invoked (see sl_FsCtl, sl_FsProgram))
- SL_ERROR_RESTORE_IMAGE_COMPLETE (Return to factory image completed, perform reset)
- SL_ERROR_ROLE_TAG_ERR (Failure to start TAG role)
- SL_ERROR_FIPS_ERR (Failure to start with FIPS mode enabled)
- SL_ERROR_GENERAL_ERR (General error during init)
\sa sl_Stop
\note Belongs to \ref basic_api
\warning This function must be called before any other SimpleLink API is used, or after sl_Stop is called for reinit the device
\par Example:
- Open interface without callback routine. The interface name and handler are
handled by the sl_IfOpen routine:
\code
if( sl_Start(NULL, NULL, NULL) < 0 )
{
LOG("Error opening interface to device\n");
}
\endcode
<br>
- Open interface with a callback routine:
\code
void SimpleLinkInitCallback(_u32 status)
{
LOG("Handle SimpleLink Interface acording to ststus %d\n", status);
}
void main(void)
{
if (sl_Start(NULL, NULL, SimpleLinkInitCallback) < 0)
{
LOG("Error opening interface to device\n");
}
}
\endcode
*/
#if _SL_INCLUDE_FUNC(sl_Start)
_i16 sl_Start(const void* pIfHdl, _i8* pDevName, const P_INIT_CALLBACK pInitCallBack);
#endif
打开文件系统不需要使用sl_Start,用sl_FsOpen打开,可以参考例程fatsd
如果我想关闭WIFI是不是只能通过sl_stop关闭?
是的
我在想能否关闭某些服务从而降低功耗,因为目前整个代码运行花费的功耗来说有一半是在这个网络服务上面
你可以参考Power Measurement例程,然后将低功耗模式添加到你的程序当中
嗯谢谢,我的理解是:
1、在Power Measurement例程中,只要设置了Power_enablePolicy();那么当所有线程进入sleep或者阻塞情况下的时候,系统会进入LPDS模式,不知道我这个理解是否正确?我在自己的开发板上做了如下测试:1、将程序中将WLAN模式设置为AP模式并通过PC连接上CC3220SF的热点,并在连接后将所有的线程置为SLEEP模式,发现总的电流还有75mA;2、不开启WLAN模式下,开启4个线程并让所有线程进入SLEEP,发现总的电流输入为11.6~15.2mA其中大部分时间保持在11.6mA,中间会有一个小波动其大小为15.2mA
2、如果上述理解正确,那是不是可以说明在simpleLink启动网络服务的模式下即使开启LPDS模式,其功耗无法限制在一个较低的水平?
你好,我查阅Power_Management代码,发现CC3220SF都是工作在STA模式下,于是我在自己的代码中将CC3220SF的工作模式从ROLE_AP切换到ROLE_STA模式后,将所有线程进入阻塞状态,此时进入LPDS。整个CC3220SF的功耗在4μA左右。但是这并不是我想要的,当CC3220SF工作在AP模式下,LPDS能否为其减少功耗呢?你们的示例代码中只展示了WLAN在STA模式下的功耗,关于其它模式的你们并没有在代码中展示出来。关于其它模式的功耗是否有文档说明?
在SimpleLink Wi-Fi® CC3x20, CC3x3x Network Processor中:
15.1.6 Power Modes versus Device Modes
The low-power policies of the SimpleLink device are only available when it is in STA and P2P client mode. Once
the device is put into AP or P2P group owner mode, the power-management profile is forced to always on.