This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHCC3235MOD: 外接3.3V电源如何配置

Part Number: LAUNCHCC3235MOD
Other Parts Discussed in Thread: CC3200, LAUNCHXL-CC3235SF

按照用户手册2.2.7.2节的步骤设置跳线后,不能正常工作。断开VBAT和BRD的跳线,芯片可以正常跑程序,但是外围电路无法供电,整体无法工作。

板子接USB和外接5V都可以正常工作。外接3.3V是,实际3.3V与地之间是3.28V左右。板子配置如下图所示:

请问该如何配置才能使得外接3.3V电源时正常工作?多谢!!!

另:2.2.7.2下的图12中,跳线是连接BRD和5V,应该是错了吧?