Part Number: CC3235SF
请问我将MQTT例程烧录进自己的板子,但是只打印了以下信息而没有连接上路由器,而将例程烧录进开发板时却可以连接上路由器,请问是什么原因造成的呢?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请问我现在已经调通了MQTT-client的wifi功能,但是我在该例程的基础上添加了IIC协议的时候,发现i2cHandle = I2C_open(CONFIG_I2C_0, &i2cParams);打不开,单独使用IIC通信的时候是可以正常使用的,但是将其添加到MQTT-client例程的时候却发现打开不了IIC,DEBUG时调到这一步时会进到faultISR(void)这里,导致程序运行不了,我看了MQTT-client例程的引脚配置,好像LED1和LED2用了IIC复用引脚,我想不要这两个LED灯,然后将该引脚复用成IIC引脚,我应该怎么处理呢,当然,我已经在syscfg里将两个LED的引脚修改了,然后添加了IIC,将SDA引脚设置为2,SCL引脚设置为1,但是我这样修改后,I2C_open()依旧打开不了。这是什么原因呢?