This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3135: cc3135&radio tool

Part Number: CC3135

TI的技术支持,您好。我在使用radio tool附带的RadioToolCLI.exe工具的时候,用一个cc3135作为tx,一个cc3135作为rx,命令分别是tx:“.\RadioToolCLI.exe -X1 -P57 -B115200 -T -z1 -c4 -m1 -w15 -n0 -t5 -v" 和rx:“.\RadioToolCLI.exe -X1 -P38 -B115200 -c4 -R -x 0123456789AB -q -d2 -t5 -v",在win10上时可以正常使用,但在win7上作为TX和RX的两个RadioToolCLI.exe工具不能同时使用,一旦两个RadioToolCLI.exe同时连接,其中一个会弹出错误对话框显示RadioToolCLI.exe已停止工作,请问是贵公司是对这方面做了限制吗?

期待您的回复。