最近买了一套CC3000+MSP430FRAM5739开发套件。在研究官方例程的时候发现一些问题,望解答
IOS上的那个SMARTCONFIG对应是哪个例程的啊,和试图接入WIFI输入的“TTT+SSDLEN+SSID+SECURTY”是相同的道理吗?
如果是,为什么我用“TTT+SSDLEN+SSID+SECURTY”可以连上无密码的,用IOS上的那个SMARTCONFIG APP却没有反映。还有,如何smartconfig上有密码的热点呀?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CC3000上的程序也需要更新之后SmartConfig才能使用。可以从这个链接下载patch programmer先更新一下:
http://processors.wiki.ti.com/index.php/CC3000_Wi-Fi_Downloads
请在https://estore.ti.com购买,或者找代理商。
在ti网上商城买的话周期应该比较长。能不能给个国内的代理商的联系方式?
您好,我是一名研究生,最近刚买了CC3000+MSP430FRAM5739的开发板,我http://processors.wiki.ti.com/index.php/CC3000_Basic_Wi-Fi_example_application_for_MSP430参考这个网页上给的DEMO学习初步开发,但是遇到一些问题,smartconfig是没有问题,在超级终端输入01,LED6闪烁,ios手机客户端一键配置之后(这个过程应该就是告诉CC3000无线密码的一个过程吧),然后LED6常亮,这就说明CC3000已经连接到我的无线网络了吗?网页上说
The example application now reboots the CC3000 device. After the reboot, the CC3000 device tries to connect to the AP detected.这一步不明白。然后我就使用08这个命令给CC3000配置IP地址,可是超级终端却给我返回illegal command,我就无法配置IP。如果我选择先配置IP,这样是可以done,可是然后再用01命令,就会是illegal command. 我实在是想不明白,该参考的都已经看过了,改更新的都更新了,这一点我可以保证,希望可以给我一个具体的有步骤的解决办法,谢谢了。