Download Driver Patch Programmer 后,LED 1+LED5+LED8,三个灯亮,LED1亮为If LED1 turns on as well, it indicates a missing MAC address. 有什么办法解决
目前我Basic Wi-Fi example application for MSP430 串口连输入03回车,没有反应
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Download Driver Patch Programmer 后,LED 1+LED5+LED8,三个灯亮,LED1亮为If LED1 turns on as well, it indicates a missing MAC address. 有什么办法解决
目前我Basic Wi-Fi example application for MSP430 串口连输入03回车,没有反应
要先download driver patch, 再download firmware patch.
然后再用02命令连上WIFI后才能用03创建socket
漏了一个,download firmware patch之后要download basic wifi application.
download 完 driver patch 和 firmware patch,在超级终端可以用哪些命令?01 / 02 / 03 /04 。。。。这些命令都代表什么意思?比如像你上面说的 “02” 是用来连接Wi-Fi,03 是用来创建 socket。
请参照http://processors.wiki.ti.com/index.php/CC3000_Basic_Wi-Fi_example_application_for_MSP430,这里有告诉这些命令的意思。