Part Number: CC3235MODS
TI工程师
您好。
我使用httpget例程进行改造。我想从我的云服务器上获取数据。请问按照下面的例程是否可以达到效果?
还有HTTPClient_connect函数得不到任何返回值。是哪里设置的不对吗?
※我对网址进行了简化处理,请见谅。云服务器地址在我自己电脑可以访问的。
#define HOSTNAME "https://private.test-api.ap-3.amazonaws.com/test"
#define REQUEST_URI "/0/dev/macaddr"
void* httpTask(void* pvParameters)
{
bool moreDataFlag = false;
char data[HTTP_MIN_RECV];
int16_t ret = 0;
int16_t len = 0;
memset(data,0,512);
ret = -1;
moreDataFlag = 1;
Display_printf(display, 0, 0, "Sending a HTTP GET request to '%s'\n",
HOSTNAME);
HTTPClient_Handle httpClientHandle;
int16_t statusCode;
httpClientHandle = HTTPClient_create(&statusCode,0);
if(statusCode < 0)
{
printError("httpTask: creation of http client handle failed",
statusCode);
}
ret = HTTPClient_setHeaderByName(httpClientHandle,
HTTPClient_HFIELD_REQ_USER_AGENT,
"x-api-key","test",strlen("test")+1,
HTTPClient_HFIELD_NOT_PERSISTENT);
if(ret < 0)
{
printError("httpTask: setting request header failed", ret);
}
ret = HTTPClient_connect(httpClientHandle,HOSTNAME,0,0);
if(ret < 0)
{
printError("httpTask: connect failed", ret);
}
ret =
HTTPClient_sendRequest(httpClientHandle,HTTP_METHOD_GET,REQUEST_URI,
NULL,0,
0);
if(ret < 0)
{
printError("httpTask: send failed", ret);
}
if(ret != HTTP_SC_OK)
{
printError("httpTask: cannot get status", ret);
}
Display_printf(display, 0, 0, "HTTP Response Status Code: %d\n", ret);
len = 0;
do
{
ret = HTTPClient_readResponseBody(httpClientHandle, data, sizeof(data),
&moreDataFlag);
if(ret < 0)
{
printError("httpTask: response body processing failed", ret);
}
Display_printf(display, 0, 0, "%.*s \r\n",ret,data);
len += ret;
}
while(moreDataFlag);
Display_printf(display, 0, 0, "Received %d bytes of payload\n", len);
ret = HTTPClient_disconnect(httpClientHandle);
if(ret < 0)
{
printError("httpTask: disconnect failed", ret);
}
HTTPClient_destroy(httpClientHandle);
return(0);
}