Other Parts Discussed in Thread: CC3220SF
三块CC3220SF评估板,一块做AP,两块做STA。
AP的IP是10.123.45.1,两个STA同时连AP的时候,绝大多数情况下IP都是10.123.45.2和10.123.45.3
但是有时会被分配成10.123.45.3和10.123.45.4
保证子网中没有其它STA连入AP,由于要用IP识别身份,这种IP分配的不确定性会导致问题
请问为什么IP分配有时会出现3和4的情况?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
三块CC3220SF评估板,一块做AP,两块做STA。
AP的IP是10.123.45.1,两个STA同时连AP的时候,绝大多数情况下IP都是10.123.45.2和10.123.45.3
但是有时会被分配成10.123.45.3和10.123.45.4
保证子网中没有其它STA连入AP,由于要用IP识别身份,这种IP分配的不确定性会导致问题
请问为什么IP分配有时会出现3和4的情况?
您好,
假设发生的情况是:站点在某个点从 AP 断开连接,然后重新连接到 AP,但由于:

这些地址不会被释放,当设备连接时,它们将被指定为0.3和.4。
详情请参阅 Network Processors guide的section 5.4。