This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3235S: I2C通信波形存在问题

Part Number: CC3235S

在用CC3235S-LAUNCHPAD烧入例程i2copt3001_cpp时,虽然通信可以成功建立,但是在测量SCL波形时,波形存在以下问题:

1、上升沿上升速度过慢

2、被CC3235S拉低的低电平并不为0,存在一个250mV的半高电平。

虽然这个现象并不影响通信,但是这是不是说明CC3235S控制I2C总线时引脚输出有一些问题呢?

同时我又测量了SDA线,发现同样存在上述两个问题,但当从机发送ACK信号或向总线写入数据时,则可以将低电平拉到0V,这说明从机对总线的控制是没有问题。