Part Number: CC3235S
尊敬的TI工程师您好
我是LAUNCHXL-CC3235S,我烧录的使out of box 例程,我在代码中设置了断点,经编译查看,读出的加速度x轴数据、加速度y轴数据、加速度z轴数据为什么都是-1呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我只是把out of box例程的link_local_task.c文件有调整。
调整的地方有:
void * linkLocalTask(void *pvParameters)
{
mq_attr attr;
int32_t msgqRetVal;
I2C_Params i2cParams;
uint8_t abb;
uint8_t abc;
char tempStr[8];
char tempStre[8];
int8_t xValRead, yValRead, zValRead;
int16_t value = 0;
int16_t valueee = 0;
float fTempRead;
/* initializes I2C */
I2C_Params_init(&i2cParams);
i2cParams.bitRate = I2C_400kHz;
i2cHandle = I2C_open(CONFIG_I2C_0, &i2cParams);
if(i2cHandle == NULL)
{
UART_PRINT("[Link local task] Error Initializing I2C\n\r");
}
/* Setup mutex operations for sensors reading */
sensorLockObj = malloc(sizeof(pthread_mutex_t));
if(sensorLockObj == NULL)
{
UART_PRINT("[Link local task] could not Setup mutex operations for sensors reading\n\r");
while(1)
{
;
}
}
pthread_mutex_init(sensorLockObj, (pthread_mutexattr_t*)NULL);
UART_PRINT("aaaaaaaaaaaaaa\n\r");
abb=accelarometerReading();
if(abb != 0) /* leave previous values */
{
UART_PRINT("nnnnnnnnnnnnnnnnn\n\r");
}
else
{
value =yValRead ;
itoa(yValRead, tempStr); //把整形转字符型函数
UART_PRINT(tempStr,8); //打印字符函数
}
#if 0
abc= temperatureReading();
if(abc != 0) /* leave previous values */
{
UART_PRINT("nnnnnnnnnnnnnnnnnnnnnnnnnnn\n\r");
}
else
{
valueee =(int)fTempRead ;
itoa((int)fTempRead, tempStre); //把整形转字符型函数
UART_PRINT(tempStre,8); //打印字符函数
}
#endif
/* initializes mailbox for http messages */
attr.mq_maxmsg = 10; /* queue size */
attr.mq_msgsize = sizeof(SlNetAppRequest_t*); /* Size of message */
linkLocalMQueue = mq_open("linklocal msg q", O_CREAT, 0, &attr);
if(((int)linkLocalMQueue) <= 0)
{
UART_PRINT("[Link local task] could not create msg queue\n\r");
while(1)
{
;
}
}
initLinkLocalDB();
/* waits for valid local connection - via provisioning task */
sem_wait(&Provisioning_ControlBlock.provisioningDoneSignal);
while(1)
{
SlNetAppRequest_t *netAppRequest;
msgqRetVal =
mq_receive(linkLocalMQueue, (char *)&netAppRequest,
sizeof(SlNetAppRequest_t*), NULL);
if(msgqRetVal < 0)
{
UART_PRINT(
"[Link local task] could not receive element from msg \
queue\n\r");
while(1)
{
;
}
}
INFO_PRINT(
"[Link local task] NetApp Request Received - handle from main "
"context AppId = %d, Type = %d, Handle = %d\n\r",
netAppRequest->AppId, netAppRequest->Type, netAppRequest->Handle);
INFO_PRINT("[Link local task] Metadata len = %d\n\r",
netAppRequest->requestData.MetadataLen);
if((netAppRequest->Type == SL_NETAPP_REQUEST_HTTP_GET) ||
(netAppRequest->Type == SL_NETAPP_REQUEST_HTTP_DELETE))
{
if(netAppRequest->Type == SL_NETAPP_REQUEST_HTTP_GET)
{
UART_PRINT("[Link local task] HTTP GET Request\n\r");
}
else
{
UART_PRINT("[Link local task] HTTP DELETE Request\n\r");
}
httpGetHandler(netAppRequest);
}
else if((netAppRequest->Type == SL_NETAPP_REQUEST_HTTP_POST) ||
(netAppRequest->Type == SL_NETAPP_REQUEST_HTTP_PUT))
{
if(netAppRequest->Type == SL_NETAPP_REQUEST_HTTP_POST)
{
UART_PRINT("[Link local task] HTTP POST Request\n\r");
}
else
{
UART_PRINT("[Link local task] HTTP PUT Request\n\r");
}
INFO_PRINT(
"[Link local task] Data received, len = %d, flags= %x\n\r",
netAppRequest->requestData.PayloadLen,
netAppRequest->requestData.Flags);
httpPostHandler(netAppRequest);
}
if(netAppRequest->requestData.MetadataLen > 0)
{
free (netAppRequest->requestData.pMetadata);
}
if(netAppRequest->requestData.PayloadLen > 0)
{
free (netAppRequest->requestData.pPayload);
}
free (netAppRequest);
}
}
static void reverse(char s[])
{
int i, j;
char c;
for (i = 0, j = strlen(s)-1; i<j; i++, j--) {
c = s[i];
s[i] = s[j];
s[j] = c;
}
}
static void itoa(int n, char s[])
{
int i, sign;
if ((sign = n) < 0) /* record sign */
n = -n; /* make n positive */
i = 0;
do { /* generate digits in reverse order */
s[i++] = n % 10 + '0'; /* get next digit */
} while ((n /= 10) > 0); /* delete it */
if (sign < 0)
s[i++] = '-';
s[i] = '\0';
reverse(s);
}
注意,在link_local_task.c文件的前面要对两个函数定义下:static void itoa(int n,char s[]);
static void reverse(char s[]);
程序烧进去后,某一个姿态数据 和 温度分别为 -1、 0,不知道问题出在哪里?