This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

launchpad(mspG2553) + cc3000boost 编译器报错,提示cstack 不足



使用的官方例程 Basic WiFi Application

在IAR(Embedded Workbench 6.5)工程中不定义 CC3000_UNENCRYPTED_SMART_CONFIG ,即使用smartconfig过程使用AES加密

编译器报如下错误

Error[e16]: Segment CSTACK (size: 0xc8 align: 0x1) is too long for segment definition. At least 0x36 more bytes needed. The problem occurred while processing the segment placement command
"-Z(DATA)CSTACK+_STACK_SIZE#", where at the moment of placement the available memory ranges were "CODE:36e-3ff"
Reserved ranges relevant to this placement:
200-223 DATA16_I
224-2cf DATA16_Z
2d0-36d DATA16_N
36e-3ff CSTACK
Error while running Linker

意思是cstack不足,查了下,是不是可以修改编译器设定的cstack大小?或者其他方法

请问如何解决? 谢谢!!