各位好:
用CC3000的smartconfig将其配置好,接入网络后,用网络调试助手和串口助手Putty相互发送数据。首先键入命令“03”,返回提示“DONE”,然后键入发送数据命令以及数据长度,AF_INET类型,目标端口,目标IP地址,键入回车,在网络调试助手上显示的信息每个数据上多了一个”3“ ?且串口助手上不显示“DONE”。具体情况附图:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你的网络调试助手上显示的是16进制的ASCII码吗?因为1的16进制就是0x31.
这个依赖于你用什么MCU, 如果忽略掉MCU的因素,CC3000可以达到6Mbps。
因为这个依赖于MCU,所以就需要case by case来看了,没有一个准确的答案。