Example App:basic_wifi_application
driver version 2.13.7.13
mcu:msp430g2553
CC3000建立tcp socket之后。
第一次发送数据能够成功,send(smtpSocket,"ST",2,0);
但是在发送完成之后wlan_tx_buffer[CC3000_TX_BUFFER_SIZE - 1] 幻数位 就会被置为为0x01. 当下次发送之后就会进入幻数检测的那个while(1)死循环里面
// The magic number that resides at the end of the TX/RX buffer (1 byte after the allocated size)
// for the purpose of overrun detection. If the magic number is overwritten - buffer overrun
// occurred - and we will be stuck here forever!
if (wlan_tx_buffer[CC3000_TX_BUFFER_SIZE - 1] != CC3000_BUFFER_MAGIC_NUMBER)
{
while (1)
;
}