This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MPS430FR5739这个芯片的编程口



TI专家好:

前一段时间因EVM板没有了,所以,这边代理商也建议我做板子,目前遇到一个问题,就是MPS430FR5739的版本数据下载接口怎么处理。

或者说,现在MPS430FR5739现在和cc3000模块spi连接完毕,MPS430FR5739和cc3000的driver等都需要通过一个接口把数据烧进去,所以

请教TI专家,这个MPS430的编程接口是哪几个,怎么使用,最好能提供一个参考的设计demo。

谢谢。

  • 你好,

    MSP430FR5739launchpad是自带仿真器,只需要连接USB接口就好。

    但是如果你是你自己做的电路板,需要引出4个管脚 RST TEST VCC GND。

    MCU采用SBW(类似JTAG下载接口)仿真,你需要一个任何MSP430系列的launchpad板作为仿真器。

    参考电路如下文档内所示: