This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3200 Networ processor 如何与M4通信?

Other Parts Discussed in Thread: CC3200

hi,

SimpleLink Host Driver文档中,对device的module不是很理解。这个device是 Networ processor与M4通信的通道吗?

在CC3200 SimpleLink™ Wi-Fi®and Internet-of-Things Solution, a Single-Chip Wireless MCU 这个文件的

Figure 1-3. CC3200 Functional Block Diagram来看,Wi-Fi Network Processor 没有与M4通信连接呀?

如果,device module是 Networ processor与M4通信的,那么SPI 或者uart口是否被内部占用了?

  • Marvin,

    您好!

    您提到的文档链接能不能提供下链接?

    CC3200是一颗SOC芯片,主要就包含了一个MCU + NWP. 这边的device应该是指SOC里MCU这块的资源,比如SPI, ADC等外设。 关于MCU M4 core与 NWP之间的链接是封闭的,您不要关心,我们所有提到的CC3200的外设,比如您提到的SPI和uart 都是您能够使用的资源,不会被占用。

    谢谢!