This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3100 Getting Started 问题

Other Parts Discussed in Thread: CC3100

你好,

我在CC3100 Getting Started 过程中,在安装USB driver 后,出现了4个COM 口,而“CC3100 SimpleLink™ Wi-Fi® and IoT Solution
Getting Started Guide“中说只会出现2个COM 口,不知道怎么回事??

还有,在论坛里看到的“CC3100里面不需要编程,直接烧写NWP的frimware",这个是怎么回事啊?是怎么操作的啊

不知道CC3100 Emulation BoosterPack这个板是用来干吗的啊??

谢谢~~~

  • 楼主,

      你在安装完USB driver以后,出现4个串口是正常现象。这主要和EVM的版本有关。早起的是2个COM口,现在的是4个。你在选择COM口进行固件刷新的时候,选择第三个。

       CC3100不是不需要编程,它是一个network processor, 它需要外接一个MCU来对它进行配置。配置的接口有UART和SPI两种。通过CC3100 emulation Boostpack这块板子主要是利用它上面的FTDI(串口转USB)来对CC3100所接的SPI flash进行固件的刷新。里面包括MAC的定义,已经相关的一些patch。

    真正的实现TCP/IP 或是UDP之类的网络通信的应用,还是在MCU端编程实现的。

    谢谢

  • 可否解释下,如何在COM口进行固件刷新啊?

    谢谢