我用的是1.12版本的Basic Wifi Application,是不是这个版本的patch programmer没有了,已经直接写在Application里了呢,另外,这个是否只是cc3000,单片机,pc三者之间的demo?还是需要配置AP?我看了教程和代码,好像LED3负责DHCP,不理解,现在程序运行到wlan_init()就运行不下去了,它是完成什么功能的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用的是1.12版本的Basic Wifi Application,是不是这个版本的patch programmer没有了,已经直接写在Application里了呢,另外,这个是否只是cc3000,单片机,pc三者之间的demo?还是需要配置AP?我看了教程和代码,好像LED3负责DHCP,不理解,现在程序运行到wlan_init()就运行不下去了,它是完成什么功能的?
请参照:http://processors.wiki.ti.com/index.php/CC3000_Wi-Fi_Downloads#Patch_Programmer
有1.12的patch programmer.
这个basic wifi application只是一个reference code, 如果开发应用的话需要自己去扩展。
配置AP是必须的。
你现在用的是什么套件?
我没有用套件,我用的5529的白色开发板和一块用于arduino平台的cc3000,我看patch programmer好像只有5739有1.12版本的。另外请问配置AP的步骤在哪看呢?我看了http://processors.wiki.ti.com/index.php/CC3000_Basic_Wi-Fi_example_application_for_MSP430F5529#Environment_Setup,我觉得应该是先patch然后environment setup然后在run the application时候再设置ap吧,也就是说只要连接了cc3000与5529以及pc,打开超级终端就应该显示一个版本号,而我现在patch无法成功,因为led3没亮,1.11版本中有一个initDriver(0)函数我过不去,不知道这个参数0是什么意思,这句话下面就是turnOn(LED3)。