This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc3000上面的一些问题



TI工程师们:

你好,我参加了TI举行的一个比赛,使用的是CC3000+TM4C123GH6PMI的开发板,参考的教程是processors.wiki.ti.com/.../China_IOT_Contest_SimpleLink_WiFi_CC3000

通过按照上面的介绍,我逐次的添加安装,但是在第二步C中也就是Rubuild it时,出现了如下的问题,希望有工程师解释说明一下:

Description Resource Path Location Type
1、File devices/lm4f120h5qr.xml does not exist. Was included by file C:/ti/CC3000SDK/CC3000 SDK/LM4F120H5QR/Basic WiFi Application/Basic WiFi Source/Basic WiFi Application CCS/Basic Wifi Application/target_config.ccxml target_config.ccxml /Basic Wifi Application line 0 Problem

2、This project was created for a device that is not currently recognized: Cortex M.LM4F120H5QR. Please go to <a href="liveaction:OpenAppCenter">CCS App Center</a> to install the device descriptor, or migrate the project to the closest match from the supported devices by adjusting project properties. Basic Wifi Application project Problems

console显示:

**** Clean-only build of configuration Debug for project Basic Wifi Application ****

"C:\\ti\\CCS\\ccsv6\\utils\\bin\\gmake" -k clean
DEL /F "Basic Wifi Application.out"
找不到 C:\ti\CC3000SDK\CC3000 SDK\LM4F120H5QR\Basic WiFi Application\Basic WiFi Source\Basic WiFi Application CCS\Basic Wifi Application\Debug\Basic Wifi Application.out
DEL /F "basic_wif_ccs.pp" "basic_wifi_application.pp" "board.pp"
找不到 C:\ti\CC3000SDK\CC3000 SDK\LM4F120H5QR\Basic WiFi Application\Basic WiFi Source\Basic WiFi Application CCS\Basic Wifi Application\Debug\basic_wif_ccs.pp
DEL /F "basic_wif_ccs.obj" "basic_wifi_application.obj" "board.obj"
找不到 C:\ti\CC3000SDK\CC3000 SDK\LM4F120H5QR\Basic WiFi Application\Basic WiFi Source\Basic WiFi Application CCS\Basic Wifi Application\Debug\basic_wif_ccs.obj
'Finished clean'

**** Build Finished ****
Buildfile generation error occurred..
This project was created for a device that is not currently recognized: Cortex M.LM4F120H5QR. Please go to CCS App Center to install the device descriptor, or migrate the project to the closest match from the supported devices by adjusting project properties.
Build stopped..


' '