This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BP-CC3301: 工具无法连接成功

Part Number: BP-CC3301


[ 4/17/2023, 18:55:49 ] Configuraton loaded successfully
[ 4/17/2023, 18:55:49 ] Avaliable options loaded successfully
[ 4/17/2023, 18:55:50 ] Device reset successfully
[ 4/17/2023, 18:55:50 ] Start 2nd Bootloader loading
[ 4/17/2023, 18:55:50 ] Loaded 6%
[ 4/17/2023, 18:55:51 ] Loaded 18%
[ 4/17/2023, 18:55:51 ] Loaded 31%
[ 4/17/2023, 18:55:52 ] Loaded 50%
[ 4/17/2023, 18:55:52 ] Loaded 63%
[ 4/17/2023, 18:55:53 ] Loaded 75%
[ 4/17/2023, 18:55:53 ] Loaded 88%
[ 4/17/2023, 18:55:54 ] Loaded 100%
[ 4/17/2023, 18:55:54 ] Container downloaded successfully
[ 4/17/2023, 18:55:54 ] Start Firmware loading
[ 4/17/2023, 18:55:54 ] Loaded 0%
[ 4/17/2023, 18:55:55 ] Loaded 0%
[ 4/17/2023, 18:55:55 ] Loaded 0%
[ 4/17/2023, 18:55:56 ] Loaded 0%
[ 4/17/2023, 18:55:56 ] Loaded 0%
[ 4/17/2023, 18:55:57 ] Loaded 0%
[ 4/17/2023, 18:55:57 ] Loaded 0%
[ 4/17/2023, 18:55:58 ] Loaded 0%
[ 4/17/2023, 18:55:58 ] Loaded 0%
[ 4/17/2023, 18:55:59 ] Loaded 0%
[ 4/17/2023, 18:55:59 ] Loaded 0%
[ 4/17/2023, 18:56:00 ] Loaded 0%
[ 4/17/2023, 18:56:00 ] Loaded 0%
[ 4/17/2023, 18:56:01 ] Loaded 0%
[ 4/17/2023, 18:56:01 ] Loaded 0%
[ 4/17/2023, 18:56:01 ] Fail download container with error Last operation <function PyXds110._secap_bulk_write at 0x000002A669604E50> return error code -1141 stopping process [ -1141 ]