This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

刚买了CC3000模块和MSP-EXP430FR5739 开发板,请教下怎么能运行起来。

Other Parts Discussed in Thread: MSP430FR5739, MSP-EXP430FR5739

TI 的工程师,你好:

我昨天刚买了CC3000和MSP-EXP430FR5739的开发板,按照《processors.wiki.ti.com/.../CC3000_Home_Automation_Application_for_MSP430FR5739》 来做, 可是走到《Step 3. Updating the Service Pack》不知道怎么做了, 请问下应该如何做。


其实我的问题很简单,就是怎样很快的把cc3000运行起来,能让我用android手机来控制就可以了,请问下应该如何做,谢谢!

  • 我认为烧写的步骤是:

    1,烧写固件。

    MSP-EXP430FR5739

    Open Start -> All Programs -> CC3000 Patch Programmer -> MSP430FR5739 -> Download Driver Patches
    LED5 and LED8 turn on upon successful completion.
    If LED1 turns on as well, it indicates a missing MAC address.   ////<----------------烧写完后 ,命令行中也没有提示任何错误,板子的LED1没有亮,板子没有任何反应

    Open Start -> All Programs -> CC3000 Patch Programmer -> MSP430FR5739 -> Download Firmware Patches 
    LED5 and LED8 turn on upon successful completion.   //《--------烧写完后,LED5和led8 也没有亮,命令行没有任何错误提示,

    2,烧写MSP430中的程序:

    Go inside "tools/MSP430Flasher_1.1.3" and run "download_cc3000_fram_Home_Automation.bat"

    其他的我就没有做什么了

    但板子没有运行起来,没有任何动作。

    请问下,应该如何做,谢谢!

  • 请问下 TI 的工程师:  我这样的烧写步骤正确吗,

    如果不正确的话,应该如何来做呢, 谢谢。

  • 自己顶一下, 我看论坛里也有很多人用CC3000,希望大家帮一下,谢谢。

  • 请再认真对一下CC3000和MSP430的方向有没有插反。

    你的操作步骤没有错。

    你再下载一个MSP430FR5739的例程,只是去把LED点亮的,跟CC3000无关的,再试试看。

    如果还是不行,我觉得有必要检查一下你的板子是不是工作的.