This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200 flash文件操作问题



TI 工程师,你们好:

        我需要在外部flash中储存一个大概500k的文件,并且需要对它进行读写操作。

例如,我从网络上获得文件保存在flash中,发现超过69000个字节左右的时候,就报错了。

于是我用C:\TI\CC3200SDK_1.0.0\cc3200-sdk\example\file_operations的例程测试,把原来限制的64Kbyte 改成69Kbyte,结果出现同意的现象。

sl_FsWrite的返回值是 -15,  

进一步查得应该是宏:#define SL_FS_ERR_OFFSET_OUT_OF_RANGE    (-15)

iLoopCnt * sizeof(gaucOldMacDonald) = 53 * 1298 = 68794
sl_FsWrite failed! -15
sl_FsClose ! 0
Error [-2006] at line [362] in function [WriteFileToDevice]


你们那个文件系统的操作函数,是不是有大小限制?

我现在必须要保存大于64K字节的文件,请帮忙解决这个问题,非常感谢。