TI工程师,你们好:
CC3200 文件系统 单个文件长度是否有限制?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我想请教一下你,用CCS UniFlash工具 Add File 一个文件到flash
Name: /test
Url:C:\Users\Administrator\Desktop\test.txt
然后我把新添加的这个/test目录以及test.txt(一个普通的txt文件,存放在电脑桌面)同步到flash,我用的是C:\ti\CC3200SDK_1.0.0\cc3200-sdk\example\file_operations这个实例,然后通过下面代码读取/test.txt
===》
#define USER_FILE_NAME_T "/test"
//#define USER_FILE_NAME_T "/test/test.txt"
//#define USER_FILE_NAME_T "/test.txt"
long lRetVal = -1;
int iLoopCnt = 0;
unsigned long READ_SIZE = 100;
unsigned long ulToken_t = 0;
//
// open a user file for writing
//
lRetVal = sl_FsOpen((unsigned char *)USER_FILE_NAME_T,
FS_MODE_OPEN_WRITE,
ulToken,
lFileHandle);
if(lRetVal < 0)
{
lRetVal = sl_FsClose(*lFileHandle, 0, 0, 0);
ASSERT_ON_ERROR(FILE_OPEN_WRITE_FAILED);
}else{
Report("open dir/file is succeed ! \n\r");
}
SlFsFileInfo_t pFsFileInfo;
sl_FsGetInfo((unsigned char *)USER_FILE_NAME_T, ulToken_t, &pFsFileInfo);
Report("pFsFileInfo.AllocatedLen:%d\n\r",pFsFileInfo.AllocatedLen);
Report("pFsFileInfo.FileLen:%d\n\r",pFsFileInfo.FileLen);
Report("-----------------------------------------------\n\r");
Report("read data: \n\r");
在终端打印的情况是下面:
==========================================================
open dir/file is succeed !
pFsFileInfo.AllocatedLen:7752
pFsFileInfo.FileLen:0
-----------------------------------------------
read data:
==========================================================
pFsFileInfo.FileLen:0--->这个文件长度居然是0,
我也尝试着改变目录读取,USER_FILE_NAME_T(就是改变这个宏所指向的路劲,经过几次尝试后,用/test这个路劲总算能打开了,但pFsFileInfo.FileLen 居然是0),请问你有碰到过,或是知道怎么解决吗?谢谢了,搞了好久了,还是没有结果,来求助了!!
TI工程师:
您好!我现在出现的问题是创建一个超过300KB的文件,编译可以通过,但是上电后起不来!比较急,谢谢!
CC3200能否创建4MB大小的文件,我的外接flash是16MB大小的。创建4MB大小文件的时候,串口打印这个调试信息[GENERAL EVENT] - ID=[60] Sender=[164]
TI工程师,你们好,
真的没有限制吗?我用CC3200创建4MB大小的文件,但是创建会失败,我的外接flash的大小是16MB。创建4MB大小文件的时候,会打印出以下调试信息
[GENERAL EVENT] - ID=[60] Sender=[164]
创建失败lRetVal = -100
希望您给个答复和建议