我是新手,请问CC3000能否实现定位功能?例如其中一个设为参考节点其他设为移动节点对其进行定位。CC3000是否需要除CCS外的软件,需要仿真器吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我是新手,请问CC3000能否实现定位功能?例如其中一个设为参考节点其他设为移动节点对其进行定位。CC3000是否需要除CCS外的软件,需要仿真器吗?
我想下载有关CC3000的例程,协议栈之类的应该到哪下?找到的都是数据手册。。还有CC3000能和TMS320F28069一起使用吗?
可以在TI的官方网站上进行下载 http://www.ti.com.cn/product/cn/CC3000/toolssoftware 是有相关软件及例程的
CC3000BOOST停产了?还有哪种CC3000的开发板有售?
建议使用TI 最新的 CC3100以及CC3200
他们和CC3000区别大吗?还有他们的例程和参考的资料多吗?
CC3000是我们的上一代NWP WIFI产品,需要外挂MCU. 有芯片也有模块.
CC3100是CC3000的升级版本,有芯片也有模块。
CC3200是我们的SOC产品,相当于M4+CC3100.
您可以看一下 TI WIKI 的资料 http://processors.wiki.ti.com/index.php/CC31xx_&_CC32xx
CC3100能和DSP的TMS320F28069一起使用吗?
可以,不过你需要移植一下CC3100 simplelink host driver.
可以参考一下http://processors.wiki.ti.com/index.php/CC31xx_Host_Interface