cc3200 sta 模式是否支持使用静态ip去连接AP
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
\code
SL_IPV4_STA_P2P_CL_STATIC_ENABLE:
Setting a static IP address to the device working in STA mode or P2P client.
The IP address will be stored in the FileSystem.
In order to disable the static IP and get the address assigned from DHCP one should use SL_STA_P2P_CL_IPV4_DHCP_SET
SlNetCfgIpV4Args_t ipV4;
ipV4.ipV4 = (_u32)SL_IPV4_VAL(10,1,1,201); // _u32 IP address
ipV4.ipV4Mask = (_u32)SL_IPV4_VAL(255,255,255,0); // _u32 Subnet mask for this STA/P2P
ipV4.ipV4Gateway = (_u32)SL_IPV4_VAL(10,1,1,1); // _u32 Default gateway address
ipV4.ipV4DnsServer = (_u32)SL_IPV4_VAL(8,16,32,64); // _u32 DNS server address
sl_NetCfgSet(SL_IPV4_STA_P2P_CL_STATIC_ENABLE,IPCONFIG_MODE_ENABLE_IPV4,sizeof(SlNetCfgIpV4Args_t),(_u8 *)&ipV4);
sl_Stop(0);
sl_Start(NULL,NULL,NULL);
\endcode