TI员工你好,我们想用vs2010模拟mcu来控制3100
1.请问3100modboost可以用vs2010单独调试吗?如果可以,怎么实现?
2.你们套件中的3100emuboost起到一个什么作用呢?只是单独的下载工具吗?vs2010模拟mcu一定要用到emuboost吗?
3.我们没有使用emuboost,而是通过一个usb转串口的小工具连接pc和3100,只使用了3100的UART1_TX,UART2_RX和p3的GND,没有接cts和rts,请问这样接可以吗?如果不行,正确的接法是怎么样的呢?
4.按照我们自己的接法,程序运行时会停在OSI_RET_OK_CHECK中,而且vs会出现异常,见附件