TI 员工,大家好:
CC3200 SDK中的函数UARTFIFOLevelSet(),功能为“Sets the FIFO level at which interrupts are generated.”。
可以设置为1/8, 1/4,1/2,7/8等,但是我看FIFO size 是16bytes, 也就是说在设置为1/8的时候,
最少要2个字节才能有中断发生。那么我想收到1个字节就发生中断该怎么做呢?
或者不用DMA方式,怎么用UART中断呢,有例程吗?
BR!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI 员工,大家好:
CC3200 SDK中的函数UARTFIFOLevelSet(),功能为“Sets the FIFO level at which interrupts are generated.”。
可以设置为1/8, 1/4,1/2,7/8等,但是我看FIFO size 是16bytes, 也就是说在设置为1/8的时候,
最少要2个字节才能有中断发生。那么我想收到1个字节就发生中断该怎么做呢?
或者不用DMA方式,怎么用UART中断呢,有例程吗?
BR!
请参考:
http://www.deyisupport.com/question_answer/wireless_connectivity/wifi/f/105/t/69121.aspx