你好,我用CC3235设计了一款设备,发现在上电的时候,MCU不能正常启动。后来我用万用表测量几个电源,发现PA的电源的电压是0.1V左右。后来我用示波器测量了电源和复位信号,发现复位信号的波形很奇怪,先是从0V上升到1V左右,等了约1秒多点,又一次上升至3V。我们电源供电电压是3V。下图是黄色是电源电压,蓝色是复位信号。
另外,我还发现,如果在上电的过程中,将MCU的某一个引脚,如TX或RX,甚至nReset接到一个较多的电压,比如电池电压或者XDS110的3.3V电压后,MCU就能顺利启动。请问这种情况有可能是哪里出了问题?