CC3200 工作在定时器捕获模式下,如何进行定时器时钟分频。
当我运行SDK中 timer_cc例程时加入
MAP_TimerPrescaleSet(TIMERA2_BASE,TIMER_A,80);//需要1M Hz时钟
捕获的数据始终是80 MHz时钟的数据。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ken
这是我修改过的定时器代码。MAP_TimerPrescaleSet直接用TimerPrescaleSet代替了
加入这个TIMER_CFG_SPLIT_PAIR TIM2应该就在TIMER_A就在16bit方式吧
MAP_TimerConfigure(TIMERA2_BASE, (TIMER_CFG_SPLIT_PAIR | TIMER_CFG_A_CAP_TIME));
TimerPrescaleSet(TIMERA2_BASE,TIMER_A,80);
//
// Register timer interrupt hander
//
MAP_TimerIntRegister(TIMERA2_BASE,TIMER_A,TimerIntHandler);
//
// Set the detection edge
//
MAP_TimerControlEvent(TIMERA2_BASE,TIMER_A,TIMER_EVENT_BOTH_EDGES);
//
// Set the reload value
//
MAP_TimerLoadSet(TIMERA2_BASE,TIMER_A,0xFFFF);
//
// Enable capture event interrupt
//
MAP_TimerIntEnable(TIMERA2_BASE,TIMER_CAPA_EVENT);
//
// Enable Timer
//
MAP_TimerEnable(TIMERA2_BASE,TIMER_A);
问题解决:
CC3200的定时器分频不是作用在定时器输入时钟上的,不管怎么分频捕获的时钟始终是80M。
它和CC2530等51内核的定时器时钟分频不一样。和STM32F1的也不一样。
分频的作用只是限定最大捕获时间。而且捕获的数据值是32Bit的,数据最高8字节始终是0,只有后面24Bit有效。