我用HttpServer例子,CC3200先自动连接AP,连接不上后,我用手机的SmartConfig设置找到CC3200设备后,能够正常访问CC3200自带的网页,但是,如果重启CC3200后,又不能自动连接刚才的那个AP了。程序是写到Flash里的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用HttpServer例子,CC3200先自动连接AP,连接不上后,我用手机的SmartConfig设置找到CC3200设备后,能够正常访问CC3200自带的网页,但是,如果重启CC3200后,又不能自动连接刚才的那个AP了。程序是写到Flash里的。
你可以看下你的程序里面有没有调用保存AP的profile的操作。
谢谢
这个函数确实是删除掉了所有的profile。你可以调用profileadd的函数来把AP的profile加上,然后connect policy设置位auto fast connect。
这样每次它都会快速重连了。
谢谢
lRetVal = sl_WlanSmartConfigStart(0, /*groupIdBitmask*/
SMART_CONFIG_CIPHER_NONE, /*cipher*/
0, /*publicKeyLen*/
0, /*group1KeyLen*/
0, /*group2KeyLen */
NULL, /*publicKey */
NULL, /*group1Key */
NULL); /*group2Key*/
这一句是连接手机SmartConfig的,是在他后面加上sl_WlanProfileAdd吗,但SSIDNAME,password从哪里得到呢
sl_WlanProfileAdd(const _i8* pName,const _i16 NameLen,const _u8 *pMacAddr,const SlSecParams_t* pSecParams ,const SlSecParamsExt_t* pSecExtParams,const _u32 Priority,const _u32 Options);
我看了一下代码,你可以不用加add profile函数,只需要将sl_WlanProfileDel()注释掉就行。
因为smartconfig会自动的得到SSID和密码,并保存这个profile。
谢谢
1、将sl_WlanProfileDel()注释掉,不要将保存的profile删除掉。
2、smartconfig会自动的得到SSID和密码,并保存这个profile。smart config配置完成SSID和密码当CC3200掉电后,都能以自动模式连接之前通过smart config保存的SSID和密码。即通过自动模式连接上AP
//set AUTO policy automatically reconnect to one of its stored profiles 自动模式下CC3200会从SPI_Flash中读取存储的profile配置AP信息并连接AP
3、lRetVal = sl_WlanPolicySet(SL_POLICY_CONNECTION,SL_CONNECTION_POLICY(1,0,0,0,1),&policyVal, 1 /*PolicyValLen*/);---设置为Auto+smartconfig的形式
Hi Ti han,
我按照你的方法在 Ti示例SmartConfig demo上注释,下载到Ti开发板上。每次重启怎么不自动连接到WiFi,而停留在sl_WlanSmartConfigStart()等待APP的配置呢?
代码如下,请指点下。
int SmartConfigConnect()
{
unsigned char policyVal;
long lRetVal = -1;
// Clear all profiles
// This is of course not a must, it is used in this example to make sure
// we will connect to the new profile added by SmartConfig
//
// lRetVal = sl_WlanProfileDel(WLAN_DEL_ALL_PROFILES);
// ASSERT_ON_ERROR(lRetVal);
//set AUTO policy
lRetVal = sl_WlanPolicySet( SL_POLICY_CONNECTION,
SL_CONNECTION_POLICY(1,0,0,0,1),
&policyVal,
1 /*PolicyValLen*/);
ASSERT_ON_ERROR(lRetVal);
// Start SmartConfig
// This example uses the unsecured SmartConfig method
//
lRetVal = sl_WlanSmartConfigStart(0, /*groupIdBitmask*/
SMART_CONFIG_CIPHER_NONE, /*cipher*/
0, /*publicKeyLen*/
0, /*group1KeyLen*/
0, /*group2KeyLen */
NULL, /*publicKey */
NULL, /*group1Key */
NULL); /*group2Key*/
ASSERT_ON_ERROR(lRetVal);
// Wait for WLAN Event
while((!IS_CONNECTED(g_ulStatus)) || (!IS_IP_ACQUIRED(g_ulStatus)))
{
_SlNonOsMainLoopTask();
}
//
// Turn ON the RED LED to indicate connection success
//
GPIO_IF_LedOn(MCU_RED_LED_GPIO);
//wait for few moments
MAP_UtilsDelay(80000000);
//reset to default AUTO policy
lRetVal = sl_WlanPolicySet( SL_POLICY_CONNECTION,
SL_CONNECTION_POLICY(1,0,0,0,0),
&policyVal,
1 /*PolicyValLen*/);
ASSERT_ON_ERROR(lRetVal);
return SUCCESS;
}
(在用例里只是注释了sl_WlanProfileDel,其他原封未动)